Skip to main content
FPicc.1
Associate III
Apr 4, 2023 9:48 PM UTC
Question

Target is not responding, retrying... - Problem debugging LoRa

Hi, I'm trying to send data via LoRa with two Nucleo wl55 boards, one receiving, and one sending. I made the code from the SubGHz_Phy_PingPong example, and altered only the process where the "ping-pong" happens. I'm trying to debug both boards, but the console keeps returning "Target is not responding, retrying..." when i run it (both together, and separately aswell). Any idea of what it could be?

Before uploading the code, the IDE also asked me to update the ST-Link on both boards, which I did, but I don't know exactly what is the propper option to update it, so I tried the HSI and HSE, but it also didn't work. Don't know if it's related too.

Appreciate the help!

This topic has been closed for replies.

3 replies

ST Technical Moderator
Apr 10, 2023 4:00 PM UTC

Hello @FPicc.1​ ,

Try replacing the USB cable, connecting under reset mode.

Check these articles for such issues, that may help:

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
Apr 10, 2023 4:59 PM UTC

Connection under reset, or with BOOT0 pulled HIGH, might provide a quick way of recovery.

Make sure you don't have any code explicitly disabling debug, or changing the debug pins functionality / assignment.

Watch also the LOW POWER modes turn OFF the chip and pins facilitating debug connectivity. Avoid going into these directly out of reset.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FPicc.1
FPicc.1Author
Associate III
Apr 20, 2023 9:35 PM UTC

I actually managed to debug the board. I had to change the last two flags in the file "sys_conf.h" from 0 to 1.

But currently I had another issue, I used this example as a base for my project, so I modified it to run as I expected (with SPI1, SPI2, RTC, ADCs, FATFS), but when I tried to debug it crashed. Eventually I found out that when I disabled all ADCs (except IN1) I could debug, but I don't know why this happens (of course, everytime I saved cubeMX I changed the flags again). Also, when I change the RTC from Binary mode, that's the default, to calendar and binary mode, the LoRa application doesn't run.

Any thoughts on this?