Skip to main content
Associate III
Jul 16, 2026 7:16 AM UTC
Solved

SWD problem STM32WL33

I have designed a custom board. I have connected SWCLK to PA3 and SWDIO to PA12. I found I can not connect. So I made a patch and connected SWDIO to PA2 which seems to be default after boot. Now I can connect to the board. However after downloading my software the board becomes unaccessible. The code is running fine on a NUCLEO-WL33CC1 board.

I can not access the board with CubeProgrammer either. It is like bricked.

I found one issue with LSE which I have connected to PB14 and PB15 instead of PB12 and PB13. So I changed my code disabled LSE and enabled LSI and tested this on a new board. Initially I can connect but as soon as I try to singlestep through the code contact is lost and after that the board is no longer accesable in CubeProgrammer either.

I am running out of boards if I can not find a way to unbrick them. ​@STTwo-32 

DirkHBest answer
Associate III
Jul 16, 2026 12:26 PM UTC

It turned out that the default setting when selecting UART in CubeProgrammer is wrong! Parity needs to be set to NONE for STM32WL33.

Now I could use the bootloader to erase the FLASH. ST-Link connects again and after some further adjustments of the cpu initialisation I am up and doing some productive work again.

Takeaway:

Never configure SWCLK and SWDIO to anything else than PA2/PA3 even though it is possible in CubeMX and according to the datasheet.

When using the bootloader set parity to NONE.

8 replies

mƎALLEm
ST Technical Moderator
Jul 16, 2026 7:41 AM UTC

Hello,

Any STM32Wxxx (STM32 wireless products) related question need to be posted in STM32 MCUs Wireless forum board.

I’m moving it.

Good luck.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
DirkHAuthor
Associate III
Jul 16, 2026 7:53 AM UTC

Thank you! I am really devastated, Have been working with STM32 for more than 10 years and never had such problem.

ST Technical Moderator
Jul 16, 2026 8:36 AM UTC

Hello ​@DirkH ,

Check whether your firmware enters Deepstop mode. 

As states in the UM3418: In deepstop mode, SWD connections and connections to STM32Tools are unavailable on STM32WL33. To program a new binary, enter bootloader mode by inserting a jumper between pins 5‑7 of the ST morpho connector CN3 and resetting the board by pressing the reset button (B4).

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
DirkHAuthor
Associate III
Jul 16, 2026 8:47 AM UTC

Hello Imen.D,

no the the software does not enter Deepstop mode. Not yet, I have to get there eventually. I am using a custom board. On the Nucleo-WL33CC1 board the software runs fine.

DirkHAuthor
Associate III
Jul 16, 2026 8:44 AM UTC

Update:

Tried to put the board into bootloader mode and connect from CUbeProgrammer. I am getting strange results on both the two boards I have programmed and also on completely new boards. Here is the log:

10:34:20 : STM32CubeProgrammer API v2.23.0 | Windows-64Bits 
10:34:25 : RTS low
10:34:25 : DTR Low
10:34:25 : Serial Port COM5 is successfully opened.
10:34:25 : Port configuration: parity = even, baudrate = 57600, data-bit = 8,                     stop-bit = 1.0, flow-control = off
10:34:25 : Activating device: OK
10:34:25 : Board       : --
10:34:25 : Chip ID: 0x95 
10:34:25 : Error: GET command not acknowledged!
10:34:25 : Reemission of Get command
10:34:25 : BootLoader protocol version: 8.2
10:34:26 : Warning: Device is under Read Out Protection
10:34:27 : Timeout error occured while waiting for acknowledgement.
10:34:27 : Error: GETID command not acknowledged!
10:34:27 : Reemission of GetID command
10:34:28 : Timeout error occured while waiting for acknowledgement.
10:34:28 : Error: GETID command not acknowledged!
10:34:29 : Reemission of GetID command
10:34:31 : Timeout error occured while waiting for acknowledgement.
10:34:31 : Error: GETID command not acknowledged!
10:34:33 : Timeout error occured while waiting for acknowledgement.
10:34:33 : Error: GETID command not acknowledged!
10:34:33 : Reemission of GetID command
10:34:34 : Timeout error occured while waiting for acknowledgement.
10:34:34 : Error: GETID command not acknowledged!
10:34:34 : Reemission of GetID command
10:34:35 : Timeout error occured while waiting for acknowledgement.
10:34:35 : Error: GETID command not acknowledged!
10:34:36 : Disconnected from device.

I attach the schematic as well. As said before I have shorted TP3 and TP1 in order to connect SWDIO to PA2. Basically connecting it to both PA2 and PA12.

DirkHAuthorBest answer
Associate III
Jul 16, 2026 12:26 PM UTC

It turned out that the default setting when selecting UART in CubeProgrammer is wrong! Parity needs to be set to NONE for STM32WL33.

Now I could use the bootloader to erase the FLASH. ST-Link connects again and after some further adjustments of the cpu initialisation I am up and doing some productive work again.

Takeaway:

Never configure SWCLK and SWDIO to anything else than PA2/PA3 even though it is possible in CubeMX and according to the datasheet.

When using the bootloader set parity to NONE.

Andrew Neil
Super User
Jul 16, 2026 1:09 PM UTC

Never configure SWCLK and SWDIO to anything else than PA2/PA3 

Never say, “never” !

There are legitimate reasons for reconfiguring those pins to other than SWD - probably the commonest is to minimise power consumption in low-power modes.

But, of course, doing this means that you can no longer use SWD - so you cannot connect via ST-Link (or any other SWD probe).

There are ways to get around this; eg,

  • Connect under Reset - the reset causes the pins to revert to their default SWD functions
  • Have a delay from power-up before reconfiguring the pins - to give time to connect
  • Provide some other trigger to “release” the pins.
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.