Suggestions on how to implement firmware upgrade on STM32WB55
Hello everyone,
I'm migrating a code base from the STM32L475 to the STM32WB55. The WB55 was selected due to availability and it's not expected to use the connectivity features (BLE, ZigBee, etc.) it has.
Looking at the OTA firmware upgrade examples for BLE/ZigBee it's not clear to me if I can use that in a project when not using the connectivity stacks.
I am still looking at AN5185 to implement something without using a wireless stack but using the firmware upgrade services.
The previous hardware (L475) had dual banks so the upgrade was implemented using one bank at a time. In the WB55 there is only one bank available, one idea is to partition this bank and allocate an amount of space to store the new image.
As a side note, the image is received using an LTE connection.
Do you have any suggestions (examples, projects, input) on implementing the firmware upgrades on the WB55?
Regards,
Carlos