Skip to main content
DS.4
Senior
Feb 7, 2024 8:50 AM UTC
Question

stopping advertisement when not advertising anymore error 0x0C

application stopped advertising , with error 0x0C, later to discover it got connected.

is this error indicates I got connected? 

does it mean other things too?

 

 

thanks

 

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
Feb 7, 2024 9:28 AM UTC

@DS.4 wrote:

application stopped advertising , with error 0x0C,


So where, exactly, did you see that error code?

From knowing what returned it, you should be able to find what it means ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
DS.4
DS.4Author
Senior
Feb 7, 2024 12:48 PM UTC

Hi @Andrew Neil 

All the document says is that:  0x0C -  Command disallowed 

Would like to know better what this means and what can it indicate on the system status.

E.g., it is disallowed (cause I am connected)  (cause I am disconnected ) ( ... .) ( .... )

 

if @ST can specify more regarding the reasons, or at least approve my reasoning for this error.

 

I opened a support ticket as well hopefully to get an answer, but if anyone already has an answer to it or a link to a document with further documentation could help a lot.

Andrew Neil
Super User
Feb 7, 2024 1:35 PM UTC

@DS.4 wrote:

All the document says is that:  0x0C -  Command disallowed 


Which document is that?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.