Skip to main content
APort
Associate III
Feb 16, 2020 2:39 PM UTC
Question

STMWB55: Flash write access during BLE connection

Hello,

We are trying to write(erase) the flash during BLE connection.

If we follow the STM32Cube_FW_WB_V1.4.0/Projects/P-NUCLEO-WB55.Nucleo/Examples/FLASH/FLASH_EraseProgram

Example the BLE connection terminates immediately (timeout error code).

Apparently you have to let the CPU2 know that you are about to access the flash. The only example I found for this is:

STM32Cube_FW_WB_V1.4.0/Middlewares/ST/STM32_WPAN/ble/mesh/PAL/STM32WB/pal_nvm.c

It works when BLE is not connected.

When there is an active connection the code is stuck in dead-loop on first:

while(LL_FLASH_IsActiveFlag_OperationSuspended());

(pal_nvm.c line 226).

Once BLE device is disconnected, it passes this while.

Now... I am trying to erase a single sector, and this happens even before address is given or anything; no prior errors.

The Erase is called from main loop handler.

CPU2 firmware used is 1.4.0 (latest).

Any ideas?

Thanks in advance.

This topic has been closed for replies.

28 replies

ST Employee
Apr 8, 2021 11:07 AM UTC

Hello,

Note that it would have been possible to have a 30ms connection interval. In that case, there would have been one page erased by interval.

Regards.

Apr 8, 2021 11:13 AM UTC

Yes, I know, but sometimes by our protocol wee need an erase 2 pages by one time.

Jonny
Associate II
Oct 25, 2021 3:27 PM UTC

Hello,

I'm currently working on an STM32WB5MMG module and while working with the BLE Mesh implementation I found something strange in the source STM provided.

On my main application I do some Write/Erase operation on flash and doing so I use all the guidelines that I found in the application notes and on this discussion.

However, I faced a problem on a part of the code that uses some libraries provided by ST for flash operation.

Sometimes (this is not something that happens all the time) my code remains stuck on this function

PalNvmErase

What I can see is that on this function there is only this check before trying to erase or write the Flash

 while( LL_HSEM_1StepLock( HSEM, CFG_HW_FLASH_SEMID ) );

I remain stuck on this while cycle

 while(LL_FLASH_IsActiveFlag_OperationSuspended());

Has this something to do with the fact that on this driver there aren't this two checks before any writing or erasing operation ?

 
cpu1_sem_status = (SemStatus_t)LL_HSEM_GetStatus(HSEM, CFG_HW_BLOCK_FLASH_REQ_BY_CPU1_SEMID);
 if(cpu1_sem_status == SEM_LOCK_SUCCESSFUL)
 
 cpu2_sem_status = (SemStatus_t)LL_HSEM_1StepLock(HSEM, CFG_HW_BLOCK_FLASH_REQ_BY_CPU2_SEMID);
 if(cpu2_sem_status == SEM_LOCK_SUCCESSFUL)

Best Regards

Jonny

ST Employee
Nov 23, 2021 7:04 PM UTC

Hello,

It is required 25ms of RF idle time to be able to erase the flash. I believe in your current setup, this is never the case and the CPU2 is blocking the flash processing.

You may use the debug GPIO in app_debug.c and check the GPIO named PES. GPIO PES is driving high by CPU2 when write/erase is blocked and low when write/erase is allowed.

Regards.