Skip to main content
Associate III
Feb 12, 2025 8:30 AM UTC
Solved

STM32WPAN extern variable error

Hi,

 

I am using a custom PCB with SM32WB5MM module. I am reading a temperature sensor and I want to update its value to the advertising package in "a_AdvData".

For this I made a "shared_variable" in my main.c (for now its just defined to 10, later it wil lstore the temperature reading from sensor).

Then I made a "extern int shared_variable;" definition in main.h.

Then in app_ble.c I assign this data to the struct of "a_AdvData" package.

Main.h

 

 

 

 

 

/* Includes ------------------------------------------------------------------*/
#include "stm32wbxx_hal.h"
#include "app_conf.h"
#include "app_entry.h"
#include "app_common.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Exported types ------------------------------------------------------------*/
/* USER CODE BEGIN ET */
extern int shared_variable;
/* USER CODE END ET */

/* Exported constants -----

 

 

 

 

 

main.c

 

 

 

 

 

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_RF_Init();
 MX_GPIO_Init();
 MX_RTC_Init();
 MX_I2C3_Init();
 /* USER CODE BEGIN 2 */

 int shared_variable = 10;

/*
 uint8_t	status;
 VL53LMZ_Configuration 	Dev;
 VL53LMZ_ResultsData 	Results;

 

 

 

 

 

app_ble.c (line 28)

 

 

 

 

 

static void Adv_Request(APP_BLE_ConnStatus_t NewStatus)
{
 tBleStatus ret = BLE_STATUS_INVALID_PARAMS;

 BleApplicationContext.Device_Connection_Status = NewStatus;
 /* Start Fast or Low Power Advertising */
 ret = aci_gap_set_discoverable(ADV_TYPE,
 CFG_FAST_CONN_ADV_INTERVAL_MIN,
 CFG_FAST_CONN_ADV_INTERVAL_MAX,
 CFG_BLE_ADDRESS_TYPE,
 ADV_FILTER,
 0,
 0,
 0,
 0,
 0,
 0);
 if (ret != BLE_STATUS_SUCCESS)
 {
 APP_DBG_MSG("==>> aci_gap_set_discoverable - fail, result: 0x%x \n", ret);
 }
 else
 {
 APP_DBG_MSG("==>> aci_gap_set_discoverable - Success\n");
 }

/* USER CODE BEGIN Adv_Request_1*/ 								//Here the values for advertising package are entered
 a_AdvData[23] = shared_variable;
/* USER CODE END Adv_Request_1*/

 /* Update Advertising data */
 ret = aci_gap_update_adv_data(sizeof(a_AdvData), (uint8_t*) a_AdvData);
 if (ret != BLE_STATUS_SUCCESS)
 {
 APP_DBG_MSG("==>> Start Fast Advertising Failed , result: %d \n\r", ret);
 }
 else
 {
 APP_DBG_MSG("==>> Success: Start Fast Advertising \n\r");
 }
 return;
}

 

 

 

 

 

  When I assign a value(instead of using "sahred_variable") to the struct inside the app_ble.c, the correct value appears in advertising package. But when I use the attached code, I get error:

./STM32_WPAN/App/app_ble.c:1030: undefined reference to `shared_variable'

So now I am confused, is there a problem that I don't see with my extern definitions or is there some linker problems?

 

My project explorer:

KlemenPfce_0-1739349093588.png

 

This topic has been closed for replies.
KlemenPfceBest answer
Associate III
Feb 12, 2025 1:44 PM UTC

Figured it out, made a function in main.c, that return the extern variable, then call it from app_ble.c. 

 

 

int update_data(void){
	return shared_variable;
}

 

1 reply

KlemenPfceAuthorBest answer
Associate III
Feb 12, 2025 1:44 PM UTC

Figured it out, made a function in main.c, that return the extern variable, then call it from app_ble.c. 

 

 

int update_data(void){
	return shared_variable;
}