Skip to main content
Filippo_MalleoBest answer
ST Technical Moderator
Apr 24, 2026 9:06 AM UTC

Hi surumadurum,

the STM32WL5 can work down to 1.8V, but if you enable the Radio end of life (EOL) monitor, via RFEOLEN bit in the PWR_CR5 register, the software stops radio activities if the VDD crosses the End-of-life low-threshold voltage (VEOLL). The latter value you can find in the datasheet, as well as the VEOLH threshold voltage.
As you can see from the datasheet, for 868 MHz the VEOLL value is 1.96 V.

For more information, you can refer to the "Radio end of life (EOL)" paragraph in the reference manual.

BR,
Filippo

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

Filippo_MalleoBest answer
ST Technical Moderator
Apr 24, 2026 9:06 AM UTC

Hi surumadurum,

the STM32WL5 can work down to 1.8V, but if you enable the Radio end of life (EOL) monitor, via RFEOLEN bit in the PWR_CR5 register, the software stops radio activities if the VDD crosses the End-of-life low-threshold voltage (VEOLL). The latter value you can find in the datasheet, as well as the VEOLH threshold voltage.
As you can see from the datasheet, for 868 MHz the VEOLL value is 1.96 V.

For more information, you can refer to the "Radio end of life (EOL)" paragraph in the reference manual.

BR,
Filippo

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
surumadurum
Associate III
Apr 24, 2026 10:53 PM UTC

Ok, thanks a lot for the clarification!

So, does that mean the bottom-line is LoRa operation is specified down to 1.8V, but only recommended above 1.96V in 868Mhz region?

 

ST Technical Moderator
Apr 27, 2026 9:46 AM UTC

Hi surumadurm,

 

the device can operate down to 1.8V, but using the radio end of life monitoring feature, it is recommended to work down to the VEOLL voltage.

 

BR,
Filippo

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks