Skip to main content
HDaou
Associate
Jul 23, 2021 12:51 PM UTC
Question

STM32WLE5JC VREFBUFF Internal Reference

I am trying to use the internal voltage reference on the STM32WL MCU. When I enable the VREBUFF, it always times out and the VREFBUF->VRR bit is not ready.

On other STM32 MCU family, I read that it is required to enable the clock for SYSCFG and VREFBUFF. But I cannot find the relevant clock for either SYSCFG or VREFBUFF in the STM32WL registers. APB1ENR and APB2ENR do not have a clock enable pin for neither.

Below is the ADC init function I am using.

On the hardware level, VREF+ is connected to VCC in my design. Would that cause a problem ? I read in the user manual section 18.2 that when VREFBUF is enabled, VREF+ pin is connected to VREFBUF. Since in my design VREF+ is connected to VCC, would that cause the problem ?

	hadc.Instance = ADC;
	hadc.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
	hadc.Init.Resolution = ADC_RESOLUTION_12B;
	hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT;
	hadc.Init.ScanConvMode = ADC_SCAN_DISABLE;
	hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
	hadc.Init.LowPowerAutoWait = DISABLE;
	hadc.Init.LowPowerAutoPowerOff = DISABLE;
	hadc.Init.ContinuousConvMode = DISABLE;
	hadc.Init.NbrOfConversion = 1;
	hadc.Init.DiscontinuousConvMode = DISABLE;
	hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START;
	hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
	hadc.Init.DMAContinuousRequests = DISABLE;
	hadc.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
	hadc.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;
	hadc.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;
	hadc.Init.OversamplingMode = DISABLE;
	hadc.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
	if (HAL_ADC_Init(&hadc) != HAL_OK)
	{
		while(1);
	}
 
 
 
	/* Start Calibration */
//	if (HAL_ADCEx_Calibration_Start(&hadc) != HAL_OK)
//	{
//		while(1);
//	}
 
 
 HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE1);
 HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);
 if (HAL_SYSCFG_EnableVREFBUF() != HAL_OK)
 {
 while(1);
 }

Thanks

This topic has been closed for replies.

1 reply

TDK
Jul 23, 2021 2:23 PM UTC

> Since in my design VREF+ is connected to VCC, would that cause the problem ?

Yes this is a problem. VREFBUF will be fighting against VCC for the pin voltage. Best case, VREFBUF doesn't work, worst case the chip is damaged.

"If you feel a post has answered your question, please click ""Accept as Solution""."