Skip to main content
Associate
May 29, 2024 9:54 AM UTC
Question

[STM32WLE5CC] MCU in standby mode and Sub-GHz radio module in listening mode

Hello, 

I have a trouble using the listening mode of the Sub-GHz radio module to wake-up the STM32WLE5CCU6 MCU from the standby mode. 

My MCU is configured to wake-up on RFIRQ (EWRFIRQ = 1).

My radio module is configured in listening mode with a 15 seconds RX period and 105 SLEEP period. All the IRQ are disabled with the Cfg_DioIrq() function except RX_DONE.

However, my MCU is wake-up (reset) each time after RX period duration (15 seconds here).

So I have the feeling that even if the "RX or TX timeout" IRQ is disabled, the IRQ is forced by the radio module and wake-up the MCU. 

 

Is there any trouble in my configuration ? Is it possible to use the listening mode when the MCU is in standby mode ? 

 

Best regards.

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Jun 27, 2024 4:35 PM UTC

Hello @MaxB1000ien 

I suggest you follow the example from this link on the STM32CubeWL. It should leave listening mode only on the next receive window.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.