Skip to main content
SLevi.1
Associate III
Jul 26, 2024 1:09 PM UTC
Question

STM32WLE5CC join accept not seen

I'm using a STM32WLE5cc inside a RAK3172 (TCXO) module on a custom board. I have custom firmware developed in the STMCube IDE. So, my join request is seen on the gateway, and the gateway sees a join accept from the server. Unfortunately the joined event is not seen on the STM. I'm using the endpoint template as a framework.

What is the best procedure to track down where the fault lies?

This topic has been closed for replies.

2 replies

SLevi.1
SLevi.1Author
Associate III
Jul 26, 2024 8:09 PM UTC

Even though the interrupts for radio rx & preamble are being setup, they are never firing. Radio tx fires ok, so the interrupt handler is ok.

STTwo-32
ST Technical Moderator
Sep 13, 2024 5:13 PM UTC

Hello @SLevi.1 

This module is using an STM32WL with the implementation of a Third party. So, I think it will be really a good idea to look for support on the Forum of the Third-Party.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.