Skip to main content
DTomi.1
Senior
May 10, 2022 4:40 PM UTC
Solved

STM32WLE5CC HSE32 TCXO input

Greetings!

I'm designing a board using STM32WLE5CCU6 MCU and decided to use a 32-MHz Clipped Sine Wave TCXO instead of a crystal for the HSE32 clock.

I have a question regarding the additional circuitry between the TCXO and MCU, is an AC coupling capacitor required? Or perhaps a load capacitor (from OSC_IN pin to GND).

The datasheet mentions to add some kind of a capacitor but I'm not sure if it's an AC cap or a load cap - "For TCXO output voltage of 0.8 Vpk-pk, 10 pF can be used."

Also what is the input impedance of the OSC_IN pin?

My TCXO is specified for a input of 10KΩ in parallel with 10 pF, am I supposed to add those externally?

I hope you can help me with these questions.

BR

Domagoj

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 10, 2022 5:15 PM UTC

In the RM0453, fig 28 and 29 you will find further hints: typically the TCXO is connected to OSC_IN via a series connection of a capacitor (e.g. 10pF) and a 220 ohms resistor, leaving OSC_OUT unused and open.

Usually, SUBGHZ_HSEINTRIMR is set to 0x00 to set the internal load capacitance to 11.3pF.

Besides this 220 Ohm series resistor, you do not need any other resistor.

Does it answer your question?

Regards

/Peter.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

5 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 10, 2022 5:15 PM UTC

In the RM0453, fig 28 and 29 you will find further hints: typically the TCXO is connected to OSC_IN via a series connection of a capacitor (e.g. 10pF) and a 220 ohms resistor, leaving OSC_OUT unused and open.

Usually, SUBGHZ_HSEINTRIMR is set to 0x00 to set the internal load capacitance to 11.3pF.

Besides this 220 Ohm series resistor, you do not need any other resistor.

Does it answer your question?

Regards

/Peter.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DTomi.1
DTomi.1Author
Senior
May 11, 2022 1:36 PM UTC

Yes, that helped. Thank you!