Skip to main content
Nando
Visitor II
Jun 16, 2024 8:52 PM UTC
Question

STM32WLE5C8U6 ADC wont start

I've been stuck trying setting up an ADC pin on an STM32WLE5C8U6 MCU for several days. Although I'm new to the ST environment, I have experience setting up ADC pins on other F series chips without any issues. Am I possibly overlooking something? According to the documentation, it appears that setting up the ADC should be even simpler on the STM32WLE5. Any guidance would be greatly appreciated.

#include "stm32wle5xx.h"

void ADC_Init(void) {
 // Enable GPIOB clock
 RCC->AHB2ENR |= (1U<<1);

 // Enable ADC clock
 RCC->APB2ENR |= (1U<<9);

 // Breakpoint here to check if ADC clock is enabled


 // Configure PB4 as an analog input
 GPIOB->MODER &= ~(3U << (2 * 4)); // Clear mode for PB4
 GPIOB->MODER |= (3U << (2 * 4)); // Set PB4 to analog mode

 // Ensure ADC is disabled before starting configuration
 if (ADC->CR & (1U<<0)) {
 ADC->CR |= (1U<<1);
 while (ADC->CR & (1U<<1));
 }

 // Breakpoint here to check if ADC is disabled

 // Enable the ADC voltage regulator
 ADC->CR |= (1U<<28);
 for (volatile uint32_t i = 0; i < 10000; i++); // Delay for voltage regulator

 // Breakpoint here to check if voltage regulator is enabled

 // Calibrate the ADC
 //ADC->CR |= (1U<<31); // Start calibration
 //while (ADC->CR & (1U<<31)); // Wait for calibration to complete
 //execution gets stuck here. If I skip calibration, execution gets stuck in the next while()
 // Breakpoint here to check if calibration is complete

 // Configure the ADC
 ADC->CFGR1 |= (1U<<3); // 10-bit resolution
 ADC->CHSELR = (1U<<4); // Select channel for PB4

 // Enable the ADC
 ADC->CR |= (1U<<0); // Enable ADC
 while (!(ADC->ISR & (1U<<0))); // Wait until ADC is ready

 // Breakpoint here to check if ADC is ready
}

uint16_t ADC_Read(void) {
	 ADC->CR |= ADC_CR_ADEN;
 ADC->CR |= ADC_CR_ADSTART; // Start conversion
 while (!(ADC->ISR & ADC_ISR_EOC)); // Wait for conversion to complete
 return ADC->DR; // Read the ADC value
}
uint16_t adcValue = 0;
int main(void) {
 ADC_Init();
 adcValue = ADC_Read();
 // Use adc_value as needed
 while (1);
}

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Jun 28, 2024 3:44 PM UTC

Hello @Nando 

I suggest you follow the configurations of this examples to implement an ADC configuration on your STM32WL MCU.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.