Skip to main content
Associate II
Feb 14, 2025 6:50 AM UTC
Solved

STM32WLE5 Module JOIN FAILED

Hi,

I'm doing tests based on the LoRaWAN_AT_Slave. One of the modules often appears tMAC txTimeOut, resulting in JOIN FAILED. Same firmware downloaded, but some devices are working, is there any doubt? Is it a hardware problem?

 

[14:47:35.933]发→◇AT+JOIN=1
□
[14:47:35.965]收←◆1s890:TX on freq 470900000 Hz at DR 0

OK

[14:47:39.965]收←◆5s893:MAC txTimeOut
+EVT:JOIN FAILED

 

This topic has been closed for replies.
ethan2Best answer
Associate II
Feb 21, 2025 8:39 AM UTC

Hi,

I have finally solved the problem, it is the hardware cause.

Thanks.

2 replies

STTwo-32
ST Technical Moderator
Feb 14, 2025 9:20 PM UTC

Hello @ethan2 

Could you please provide more details. What is the exact module you are using (a third party module or a module based on your own design), what is the code you are using and all your use case details if possible.

Best Reagards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ethan2AuthorBest answer
Associate II
Feb 21, 2025 8:39 AM UTC

Hi,

I have finally solved the problem, it is the hardware cause.

Thanks.