Skip to main content
YDOVG.11
Associate II
Mar 15, 2023 4:55 PM UTC
Solved

STM32WLE5 high current consumption in Stop2 (RAK3172-SIP)

Hello

I am trying to implement low power mode with STM32WLE5 MCU (as a part of RAK3172-SIP).

However, the current consumption is unreasonably high.

I measure around 200uA with 3.6V and around 150uA with 3.3V.

Did many tests with different configurations, checked the RF switches. I use TXCO, but even if I run with internal clock - no changes. Debug mode is disabled.

How can I debug it further?

I even tried to go into Stop2 mode directly before HAL_Init() - still the same 200uA (at 3.6V) consumption. So even before all periphery is initialized I cannot get the lower consumption.

I did similar test with Wio-e5 module just to check that the HW is not an issue, and there I 've got around 300uA (at 3.6V). So I have no questions to HW.

Regarding the HW, there I have one 100k resistor to BOOT0 to GND and one 100k pullup to nRST. The rest is caps and inductors for supply lines, nothing else is connected to the module.

I was thinking this is because of SMPS - but I checked that it is not running in Stop2.

Please guide me how to debug this.

This topic has been closed for replies.
YDOVG.11
YDOVG.11Best answer
Associate II
Mar 16, 2023 10:26 AM UTC

Well.... I found the reason why the consumption was too high.

The simple answer RTC.

If you configure date/time, alarm and timestamp in MX_RTC_Init then the consumption will be on those 200uA.

Seems like one should not initiate alarms or date.

Now I am around 1.5uA.

1 reply

YDOVG.11
YDOVG.11AuthorBest answer
Associate II
Mar 16, 2023 10:26 AM UTC

Well.... I found the reason why the consumption was too high.

The simple answer RTC.

If you configure date/time, alarm and timestamp in MX_RTC_Init then the consumption will be on those 200uA.

Seems like one should not initiate alarms or date.

Now I am around 1.5uA.