Skip to main content
DTomi.1
Senior
Oct 20, 2022 3:33 PM UTC
Question

STM32WLE5 frequency deviation for FSK modulation

Greetings,

what is the recommended frequency deviation parameter for the FSK modulation with 250 kbps bitrate?

Or rather what is the dependency of RX sensitivity in relation to the FSK_FDEV parameter?

I can see that the limitation is to have the modulation index > 0.5, so in this case that would mean that FSK_FDEV > 62.5 kHz and also the limitation is on BW, so FSK_FDEV < 125 kHz.

In that range, what FSK_FDEV will give me the best RX sensitivity?

Best regards,

Domagoj

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Oct 20, 2022 3:49 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..