Skip to main content
Associate III
Dec 17, 2025 5:08 AM UTC
Question

STM32WLE5 Errata issue-"TX spurs around carrier at a multiple of HSE clock frequency"

Hi ,

we are using LORA , 22 dBm , 3.3V system , TX and RX path are connected via RF SWITCH on Board . 

we see minor Sensitivity Degradation  of 1-2 dB only around the  HSE 32 Mhz clock multiple. ( Sensitivity of the stm32wle5 receiver path )

I have several questions regarding this Errata issue:

1. Does the SPUR issue happen only in TX Mode or also in RX mode of the stm32wle5 ?

2. If it relates also to RX mode - cause this spur be the cause of the sensitivity degradation of the stm32wle5 ?

 

Thank you,

Viola