Skip to main content
WCaet
Associate
May 29, 2023 1:05 AM UTC
Question

stm32wle5 cubeide lorawan 1.3.0 with custom board change data rate

Hi all.

I'm working with stm32wle5 (rak3172 module) with a custom board.

It works but now I need to change default data rate DR_2 to DR_0 (need to increase distance).

I have already tried to change the lines below at file RegionAU915.h

​

//Minimal datarate that can be used by the node

#define AU915_TX_MIN_DATARATE           DR_0

​

//Default datarate used by the node

#define AU915_DEFAULT_DATARATE           DR_0 //DR_2

​

//The minimum datarate which is used when the dwell time is limited.

#define AU915_DWELL_LIMIT_DATARATE         DR_0 //DR_2

​

Also I have set ADR to off.

Even with this changes the endnode keeps using DR_2.

I appreciate any help.

This topic has been closed for replies.