Skip to main content
Associate III
Aug 3, 2025 10:39 AM UTC
Question

stm32wle5 bga package - output return loss measurement(tx mode)

Hi ,

 

I am trying to measure the output return loss ( in tx mode) of my board rf chain which include the stm32wle5.

if i understnad correctly - in order to do that i need to put the STM32WLE5  in TX MODE which means its PA should be powered up and ready to transmit but without any transmitted data.  ( so that i will be able to measure the Return loss using external VNA connected to the TX RF PORT of my board)

is there an option to do that ?  i cant seem to find a way to make the internal PA ready to transmit (powered up) without actually transmitting .   is it possible to measure the output RL as i described ?

 

thank you,

viola

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Sep 19, 2025 2:53 PM UTC

Hello @viola 

May i know why are you interested in this? Are you experiencing unsatisfactory TX performance that is far from what is stated in the datasheet?

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.