Skip to main content
moatjon
Associate II
Nov 17, 2021 3:04 PM UTC
Question

STM32WLE timing between OTAA request and gateway response

Hi All,

I'm creating a TTN application using a STM32WLE5JC. After configuring the LoRaWAN application in STM32CubeIDE I have been able to send an OTAA join request to a gateway using the credentials provided by the TTN application. I can see the join request being accepted in the TTN console and I can also see the radio activity in SDRsharp.

My problem is the following:

Even though the TTN application accepts my OTAA request, my LoRa application on the STM32 always end up with a "MAC txTimeOut" message over the debug trace output. I can see that this message always appears 4 seconds after the OTAA Tx. Looking at the TTN console and the local radio activity, I can see that the gateway does in fact respond, but it takes about 5 seconds.

My assumption is that the gateway takes longer to reply to the join request, and that the STM32 thus ignores this late reply.

Some more information:

  • I am using the 868 MHz EU band.
  • The TTN application uses MAC V1.0.3
  • The 4 second trace message corresponds to 4 actual seconds passing, i.e. the message timestamp is correct.

This issue may be related to this issue and/or this issue. There seem to be quite some discussion on the TTN forums which mention that the join delay should indeed be around 6 seconds.

Can anybody tell me what the root of this problem can be? Is this an issue with my device configuration, TTN configuration or something different?

Any help is much appreciated!

This topic has been closed for replies.