Skip to main content
JDave.4
Associate III
Sep 2, 2025 5:20 AM UTC
Question

STM32WL5MOC LoRaWAN_AT_Slave

Hello,

I would like to use STM32WL5MOC module with AT Slave interface. In STM32WL package:

* Which FW is recommended for STM32WL5MOC module: Single core(
LoRaWAN_AT_Slave) or dual core(LoRaWAN_AT_Slave_DualCore)?

* I couldn't find any examples for master/host MCU. Is there any example demonstrating how to configure the device using AT commands for any STM32 MCU as host?  

Thanks.

This topic has been closed for replies.

4 replies

JDave.4
JDave.4Author
Associate III
Sep 20, 2025 7:34 AM UTC

Any suggestion?

STTwo-32
ST Technical Moderator
Sep 26, 2025 2:46 PM UTC

Hello @JDave.4 

For your implementation, i suggest you have a look at the LoRaWAN_AT_Slave example. it is made to be used with a host communicating throw UART. The host can be a PC or a Programmed MCU.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JDave.4
JDave.4Author
Associate III
Sep 30, 2025 7:34 AM UTC

Hello,

I will use that example but it is only for module FW. What about host MCU example? Which AT commands must be used by host in which sequence? 

STTwo-32
ST Technical Moderator
Oct 1, 2025 7:17 AM UTC

There is not a host MCU example developed. What you should do is developing the FW of the Host using the AT commands (available on the chapter 14 of the AN5406). For the sequence, you may follow the same sequence of commands as on theLoRaWAN_End_Node.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.