Skip to main content
User2501
Associate II
Jan 20, 2025 10:39 AM UTC
Solved

STM32WL5MOC bootloader mode

Hello, 


I'm looking for advices to place the module STM32WL5MOC in bootloader mode from different methods :

  • Through BOOT0 and NRST but I can not find the communication interface that I can communicate with (for example UART) this specific mcu in the application note AN2606.
  • Also, I'm interested to know how can I access to the new firmware stored in the External memory flash for firmware update as the flash that is in the dev board B-WL5M-SUBG1 using as an example.
  • Is it possible to place this module in bootloader mode in the software if I can not have access to the BOOT0 and NRST from an external device that can control it?
  • Any example to do FUOTA point to point if I want to use the SubGHz modulation and not LoRaWAN server?

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 24, 2025 1:42 PM UTC

Hello @User2501 

  • The STM32WL5MOC is a module based on the STM32WL55JC. So, you can find all details on boot operation for this module on the chapter 84 of the AN2606. 
  • Unfortunately, there is not such an example on a board that include the STM32WL.
  • Follow the Pattern 13 of the table 2 of the AN2606 to know how to that.
  • There is not a P2P FUOTA application, you can use the LoRaWAN implementation and try to build your own in a P2P context. 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Feb 24, 2025 1:42 PM UTC

Hello @User2501 

  • The STM32WL5MOC is a module based on the STM32WL55JC. So, you can find all details on boot operation for this module on the chapter 84 of the AN2606. 
  • Unfortunately, there is not such an example on a board that include the STM32WL.
  • Follow the Pattern 13 of the table 2 of the AN2606 to know how to that.
  • There is not a P2P FUOTA application, you can use the LoRaWAN implementation and try to build your own in a P2P context. 

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.