Skip to main content
HVeer.1
Associate II
Jan 26, 2022 3:52 PM UTC
Question

STM32WL55JC1 LoRa Timeout Issue

We are also facing same tx timeout in our custom designed hardware. We are using XO clock in the design and donot have option for TCXO. Please share your inputs whether STM32WL55JC1 will work with XO clock. We got struck with TX Timoeut issue.

0693W00000JNQ9LQAX.png

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Jan 26, 2022 5:01 PM UTC

DNP, are you sure it starts promptly? Time the startup, ie ON to READY

Semtech's timeouts tend to be all encompassing. Perhaps work the logic so you spin up the clock separately, and turn it off under a different activity (lack-of) timeout.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Dana Myers
Senior
Jan 26, 2022 5:59 PM UTC

STM32WLxx has on-chip load capacitors and shouldn't need C34/C48 to be populated, but it will need, as @Mike_ST​ mentions, the on-chip capacitors to be set. Of course, they're part of the SubGHz radio, which is glommed on to HSE.

Indeed, TxTimeout is likely the result of the HSE starting very slowly or not at all (probably the case).

Mike_ST
ST Technical Moderator
Jan 26, 2022 5:49 PM UTC

Hello,

Not sure this is the problem you are facing, but you might have to do some calibration.

The AN5042 describes how to set the SUBGHZ_HSEINTRIMR (REG_XTA_TRIM) and SUBGHZ_HSEOUTTRIMR (REG_XTB_TRIM) registers when not using a TCXO.

Please have a look.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
HVeer.1
HVeer.1Author
Associate II
Jan 29, 2022 5:15 AM UTC

Hello,

Thanks for your inputs. I did the following configuration XTAL_DEFAULT_CAP_VALUE as 0x19.

    SUBGRF_WriteRegister( REG_XTA_TRIM, XTAL_DEFAULT_CAP_VALUE );

    SUBGRF_WriteRegister( REG_XTB_TRIM, XTAL_DEFAULT_CAP_VALUE );

With this, class A / C & Class C FUOTA works good. but class b still having inconsistent functioning and class b FUOTA does not started work at all.

Note : Class B / Class B FUOTA works good on nucleo-wl55jc1 hardware, it uses TCXO.

Please share your inputs.

Thanks,

Hariharan.V.

VChau
Associate II
Apr 27, 2022 7:06 PM UTC

Hello I am starting a workover on stm32wljc1 i need a base code for this where should I go

​