STM32WL55JC Flash locked after using LoRaWAN_End_Node_DualCore from STM32Cube_FW_WL_V1.1.0
Hi,
I wanted to update from version 1.0.0 to 1.1.0 and after flashing the LoRaWAN_End_Node_DualCore demo on my Nucleo WL55JC, I cannot take control over the device anymore.
I can connect with a debugger on CPU1 and access registers, but memory is only read as zeroes. CPU1 is in constant Hardfault, and I cannot modify the Flash in any way.
It seems that CPU2 security is activated and I cannot find a way to disable it, same for any security options. I'm using CubeProgrammer 2.8
RDP = 0xFF
ESE = 1
FSD = 0
DDS = 1
HDPAD = 0
If there is a way to recover this board I would be very grateful.
Thank you
BC