Skip to main content
SeppeBudenaers
Associate II
Mar 3, 2025 11:55 AM UTC
Solved

STM32WL55CCUX LoRa endnote skeleton not compiling

Hi, I am trying to implement a LoRa endnote skeleton on my STM32WL55CCU. I have tried a lot of different ways of generating the project but I always run into errors. I think its due to the way the code generates because the structure doesn't resemble at all the LoRa endnote Example from the nucleo wl55jc1. I also ran into a lot of problems generating the LoRa endnote Example, it can only be done through the IDE if you use MX it doesn't work.

Screenshot 2025-03-03 113314.png

So my question is there somewhere a STM32WL55CCU LoRa endnote skeleton I can download and start modifying or what am I doing wrong ? 

Thank you in advanced for your reply :)

Seppe Budenaers

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Mar 3, 2025 1:07 PM UTC

Hello @SeppeBudenaers 

Unfortunately, the example is not available based on STM32WL55CCU since there is not any ST Evaluation board based on this MCU. So, I suggest you start your project using the STM32WL55CCU MCU and on the .ioc file of this project, set the same configuration as on the .ioc file of the Nucleo-WL55JC example. After that, you can refer to the .c/.h files of the example to know what you should add to your generated project (the structure difference should not be an issue). 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Mar 3, 2025 1:07 PM UTC

Hello @SeppeBudenaers 

Unfortunately, the example is not available based on STM32WL55CCU since there is not any ST Evaluation board based on this MCU. So, I suggest you start your project using the STM32WL55CCU MCU and on the .ioc file of this project, set the same configuration as on the .ioc file of the Nucleo-WL55JC example. After that, you can refer to the .c/.h files of the example to know what you should add to your generated project (the structure difference should not be an issue). 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.