Skip to main content
Son, Dong-Seong
Associate III
Nov 22, 2021 4:01 AM UTC
Question

STM32WL55CCU6 : how to receive Uart1 data

Hi

I am testing STM32WL55.

I am testing UART1 of STM32WL55 by referring to SubGHz_Phy_PingPong​

I can transmit data using UTIL_ADV_TRACE_Send.

​I tried to receive data from terminal using UART1.

But it didnot work.

​

I inserted UTIL_ADV_TRACE_StartRxProcess(TRACE_RxCpltCallback); in SystemApp_Init();

TRACE_RxCpltCallback is as belows

​

void TRACE_RxCpltCallback(uint8_t *PData, uint16_t Size, uint8_t Error)

{

UTIL_ADV_TRACE_Send(PData, Size);

}

​

When data is input from the terminal, no data is returned.​

When a break point is set in the TRACE_RxCpltCallback function, a break is not caught when inputting data.

When I set HAL_UART_RxCpltCallback function, a break is caught in

HAL_UART_RxCpltCallback function when inputting data

​

When inputting data, Should TRACE_RxCpltCallback run when data is entered? Or should HAL_UART_RxCpltCallback work?

Let me know that.

Please Let me eplain how to resolve the problem if there are other problems or not

​

​1. SystemApp_Init() function

​void SystemApp_Init(void)

{

  /* USER CODE BEGIN SystemApp_Init_1 */

// Ensure that MSI is wake-up system clock

__HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI);

// Initialize timer and RTC

UTIL_TIMER_Init();

// Initialize the terminal

UTIL_ADV_TRACE_Init();

UTIL_ADV_TRACE_RegisterTimeStampFunction(TimestampNow);

// Set verbose LEVEL

UTIL_ADV_TRACE_SetVerboseLevel(VERBOSE_LEVEL);

/*Init low power manager*/

UTIL_LPM_Init();

/* Disable Stand-by mode */

UTIL_LPM_SetOffMode((1 << CFG_LPM_APPLI_Id), UTIL_LPM_DISABLE);

UTIL_ADV_TRACE_Send("TEST\r\n", 6);

UTIL_ADV_TRACE_StartRxProcess(TRACE_RxCpltCallback);

  /* USER CODE END SystemApp_Init_1 */

}

2. SubghzApp_Init() function

void SubghzApp_Init(void)

{

 /* Radio initialization */

  RadioEvents.TxDone = OnTxDone;

  RadioEvents.RxDone = OnRxDone;

RadioEvents.TxTimeout = OnTxTimeout;

  RadioEvents.RxTimeout = OnRxTimeout;

  RadioEvents.RxError = OnRxError;

  Radio.Init(&RadioEvents);

  /* USER CODE BEGIN SubghzApp_Init_2 */

  Radio.SetChannel(RF_FREQUENCY);

  Radio.SetTxConfig(MODEM_LORA, TX_OUTPUT_POWER, 0, LORA_BANDWIDTH,

           LORA_SPREADING_FACTOR, LORA_CODINGRATE,

           LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,

           true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);

  Radio.SetRxConfig(MODEM_LORA, LORA_BANDWIDTH, LORA_SPREADING_FACTOR,

           LORA_CODINGRATE, 0, LORA_PREAMBLE_LENGTH,

           LORA_SYMBOL_TIMEOUT, LORA_FIX_LENGTH_PAYLOAD_ON,

           0, true, 0, 0, LORA_IQ_INVERSION_ON, true);

  Radio.SetMaxPayloadLength(MODEM_LORA, MAX_APP_BUFFER_SIZE);

  /*calculate random delay for synchronization*/

  random_delay = (Radio.Random()) >> 22; /*10bits random e.g. from 0 to 1023 ms*/

  /*fills tx buffer*/

  memset(BufferTx, 0x0, MAX_APP_BUFFER_SIZE);

  APP_LOG(TS_ON, VLEVEL_L, "rand=%d\n\r", random_delay);

  /*starts reception*/

  Radio.Rx(RX_TIMEOUT_VALUE + random_delay);

  /*register task to to be run in while(1) after Radio IT*/

  UTIL_SEQ_RegTask((1 << CFG_SEQ_Task_SubGHz_Phy_App_Process), UTIL_SEQ_RFU, RF_Process);

  /* USER CODE END SubghzApp_Init_2 */

}

3. MX_SubGhz_Phy_Process() function

void MX_SubGHz_Phy_Process(void)

{

  /* USER CODE BEGIN MX_SubGHz_Phy_Process_1 */

UTIL_SEQ_Run(UTIL_SEQ_DEFAULT);

  /* USER CODE END MX_SubGHz_Phy_Process_1 */

}

This topic has been closed for replies.