Question
STM32WL55: High consumption by RF section
- 6 replies
- 1206 views
Hello.
I'm using the Nucleo-WL55JC board with LoRaWAN End-Device firmware (US915 region).
To measure the current consumption of the RF section, I removed the JP2 (I_RF) jumper (as per the manual) and connected an ammeter.
The issue is that the RF section consumes around 80mA during reception, and the power consumption during transmission is also significantly higher than the datasheet values.
I checked the FE_CTRL_1 to FE_CTRL_3 signals, and they look correct. The SMPS output is about 1.5V, which seems fine.
However, as I understand it, the RF section's current consumption should not exceed 5mA during reception.
What can be wrong?
Measurements are attached.