Skip to main content
FAlpa.1
Associate
Jul 13, 2023 5:12 PM UTC
Solved

STM32WL55 Dual core debug problem

Hello
friends, I am trying to make a dual core example on the Wio-E5 STM32WLE5JC Module. I made all the settings as in this video.  However, only CM4 works when debugging. CM0PLUS is not working and I am getting this error Target unknown error 32

Error in initializing ST-LINK device.
Reason: Unknown. Please check power and cabling to target. I tried this on STM32Cube ide 1.7.0 and 1.8.0.

This topic has been closed for replies.
IIRHO.1
IIRHO.1Best answer
ST Employee
Jul 14, 2023 8:28 AM UTC

Hello @FAlpa.1  and welcome to ST Community .

Wio-E5 is based on the STM32WLE5JC wish use just a single core ( Cortex-M4 ). you can't use it with a dual core application. I suggest you try an STM32WL5XXX for a dual core application.

I hope this is helpful.

Issam

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

IIRHO.1
IIRHO.1Best answer
ST Employee
Jul 14, 2023 8:28 AM UTC

Hello @FAlpa.1  and welcome to ST Community .

Wio-E5 is based on the STM32WLE5JC wish use just a single core ( Cortex-M4 ). you can't use it with a dual core application. I suggest you try an STM32WL5XXX for a dual core application.

I hope this is helpful.

Issam

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.