STM32WL55 can't change FSK Data rate.
I use the wl55 on the nucleo kit, with the ping pong exemple (one core but same with 2) in subghz_phy_app.h i change the define for
#elif (( USE_MODEM_LORA == 0 ) && ( USE_MODEM_FSK == 1 ))
#define FSK_FDEV 10000 /* Hz */
#define FSK_DATARATE 10000 /* bps */
#define FSK_BANDWIDTH 399000 /* Hz */
#define FSK_PREAMBLE_LENGTH 50 /* Same for Tx and Rx */
#define FSK_FIX_LENGTH_PAYLOAD_ON false
Changing value of FSK_DATARATE don't change data rate on air which stay at about 6800bds (i have try from 50000 to 1000 with the same result)
changing FSK_FDEV change effectivly the spectrum.
i use Gnuradio for these tests.
As far as i can debug trace every thing appear normal, on the subghz SPI 0x8A and 0x8B packet seem correct.
Where and what is the problem ?
JP