Skip to main content
Associate II
Mar 3, 2026 2:46 AM UTC
Solved

STM32WL3x reference design - downloading program

Starting my design on a reference design based on STDES for WL3 series. I would like to know what is needed for the smallest hardware connection to download a program from ST32CUBE IDE. I need to have the minimum amount of connectors on the board. I.E. I don't want to plug in my board that I designed to the NUCLEO base board debugger for downloading  a program if I don't have to.  Can I take advantage of the STDC14 connection on the ref Des and if so, do I need some external piece of hardware to connect to it which then connects to the USB port on a computer?  Thanks!

TDK
TDKBest answer
Mar 5, 2026 2:02 AM UTC

A few things:

  • You need a programmer such as STLINK-V3MINIE | Tool - STMicroelectronics
  • You need to power the board independently of the programmer.
  • At a minimum, you need to connect GND, SWDIO and SWCLK between the board and the programmer. Sometimes VCC is also needed if the programmer has a level shifter.

Typically it's better to use a standard header like the STDC14 connector and place that on your board instead.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

KB1DCAuthor
Associate II
Mar 5, 2026 1:40 AM UTC

Can anyone reply to this question?

 

TDK
TDKBest answer
Mar 5, 2026 2:02 AM UTC

A few things:

  • You need a programmer such as STLINK-V3MINIE | Tool - STMicroelectronics
  • You need to power the board independently of the programmer.
  • At a minimum, you need to connect GND, SWDIO and SWCLK between the board and the programmer. Sometimes VCC is also needed if the programmer has a level shifter.

Typically it's better to use a standard header like the STDC14 connector and place that on your board instead.

"If you feel a post has answered your question, please click ""Accept as Solution""."