Skip to main content
CEagl.1
Associate II
Nov 26, 2024 1:36 PM UTC
Solved

STM32WL33 specification

Hi,

I am looking to use the STM32WL33 in a product. 
I am curious as to what the chip is in terms of its silicon. Is the M0+ equivalent to an available MCU?
What is on the radio side? Is this an S2-LP for example?

Thanks

This topic has been closed for replies.
Philippe SIMONNET
ST Employee
Nov 26, 2024 3:09 PM UTC

Hello,

regarding Radio IP, this is an evolution of S2-LP radio, but not the same.

let's say better performance/power consumption and new features. and if you are familiar with S2-LP you won't be lost

;)

Philippe

4 replies

Andrew Neil
Super User
Nov 26, 2024 1:44 PM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
CEagl.1
CEagl.1Author
Associate II
Nov 26, 2024 1:54 PM UTC

Thanks for the links. The second one was very useful as it links to reference designs, which i was struggling to find.
However. It doesnt answer my initial question.

The reason i am asking is that this chip as far as i am aware is brand new. As such there isnt much info on it working besides some examples. 
If it is based on an already existing radio, i.e the S2-LP then it may be a bit easier to work with.
Many manufacturers do this. For example Texas Instruments uses the CC1101 Transceiver in most of their sub ghz SOC.

Not just that, but i like to know what i am working with. If this is brand new silicon. It usually comes with issues.

STTwo-32
ST Technical Moderator
Nov 26, 2024 2:38 PM UTC

Hello @CEagl.1 

Thank you so much @Andrew Neil for your contribution. to understand more about the STM32WL33 radio part, I suggest you take a look at the chapter 29 of RM0511.If you are looking for more specific details, you need to contact an FAE or one of our Sales & marketing teams. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.