Skip to main content
CEagl.1
Associate II
Nov 28, 2024 12:50 PM UTC
Question

STM32WL33 QSPI VS SPI

Hi 
I am hoping someone might be able to help me with some calculations.

I am assessing the STM32WL33 for use in a product.
One of the peripherals will be an EEPROM, an M95P32.

The EEPROM supports Dual/Quad Output (Read) However the STM32 does not appear to have a hardware QSPI.

So i am trying to determine whether to implement a Quad Read in software (bitbanging).

Can anyone help me to understand the max data transfer on 4 wire SPI using hardware, Vs that of Quad Read using software.

 

Many thanks 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Dec 23, 2024 4:37 PM UTC

Hello @CEagl.1 

I suggest you test both of them, but I personally think that the SPI will do better since it does not depend on the overhead of software execution and the maximum speed is limited by the GPIO toggling rate and the processing speed of the microcontroller.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.