Skip to main content
machinehum
Associate II
May 8, 2026 9:12 AM UTC
Question

STM32WL33 Deepstop power consumption higher than normal

We have a custom `STM32WL33CCV6` (`VFQFPN32`) board that should reach about `4 µA` in Deepstop, similar to the NUCLEO-WL33, but instead it drops only to roughly `450–500 µA` and appears to restart on Deepstop entry. `NRST` does not glitch low, and the behavior is unchanged with only `3.3V` and `GND` connected. We also tested direct `HAL_PWR_EnterDEEPSTOPMode()` with wake sources disabled, and it still appears to reboot rather than stay in Deepstop.

We reviewed ST errata `ES0612` and applied the documented `VFQFPN32` workaround from section `2.2.9` for nonbonded GPIOs causing increased Run-mode current by forcing the listed nonbonded pins to pulldown at startup. That workaround had no effect on the Deepstop issue. The custom board’s `VFBSD / VLXSD / VDDSD / VDDRF` schematic and BOM appear close to the ST reference, so we are asking whether there are known WL33 low-power / SMPS / Deepstop pitfalls beyond errata `2.2.9` that could explain a persistent `~500 µA` floor or an apparent reset/restart on Deepstop entry instead of the expected `~4 µA`.

It almost seems like deepstop is resetting the pins to their reset value or something??

2 replies

Andrew Neil
Super User
May 8, 2026 9:32 AM UTC

@machinehum wrote:

We have a custom `STM32WL33CCV6` (`VFQFPN32`) board ??


Then you'll need to share your schematic!

How to write your question to maximize your chances to find a solution

 

Are you measuring with your ST-Link (or whatever) physically disconnected, and have you done a full power cycle (not just a reset) before measuring?

 


@machinehum wrote:

similar to the NUCLEO-WL33??


Do you achieve 4uA on the Nucleo board?

 


@machinehum wrote:

schematic and BOM appear close to the ST reference


How close is "close" ... ?

You need to show the schematic for people to be able to check!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
machinehum
Associate II
May 11, 2026 6:22 AM UTC

Hey thanks for the reply. Yes we got 4uA on the devboard, stlink is completely disconnected, we're measuring right on the 3.3V bus, attached is schematic. Please note U2, R2, R3 are nopop.