Skip to main content
Associate
Sep 16, 2025 8:02 AM UTC
Solved

STM32WL30 change USART baud rate

Hello everyone,

I'm working with the STM32WL30 and I'm trying to change the baud rate of the USART peripheral. However, I'm encountering some issues when I change the baud rate.

The function I wrote for changing the baud rate looks like this:

void changeBaudRate(uint16_t baudRate) {
 // start USART reset
 RCC->APB1RSTR |= RCC_APB1RSTR_USARTRST;
 // disable interrupt
 NVIC_DisableIRQ(USART1_IRQn);
 // stop reset
 RCC->APB1RSTR &= ~RCC_APB1RSTR_USARTRST;

 // set BRR
 USART1->BRR = 16000000 / baudRate;
 // set CR1
 USART1->CR1 = USART_CR1_RXNEIE_RXFNEIE | USART_CR1_TE | USART_CR1_RE | USART_CR1_UE;

 // set IR prio
 NVIC_SetPriority(USART1_IRQn, 1);
 // enable IR
 NVIC_EnableIRQ(USART1_IRQn);
}

  

When I configured the baud rate for the first time, everything works fine and I receive the messages. If I change the baudrate to another value, I won't receive messages on the new baud rate, but still with the previously configured baud rate. When I debug the baud rate change, I can see, that the BRR was changed to the new value, but somehow the peripheral still uses the previous BRR value.

 

I also used this logic with a STM32G0 controller without any problems.

 

Thank you in advance for your help!

Best regards,
Philipp

This topic has been closed for replies.
PhilippRBest answer
Associate
Sep 16, 2025 2:37 PM UTC

I found the problem. The software which I used for testing the USART interface was not working as I expected it to do. So the baud rate of the controller was indeed configured back to the initial value. I modified the test software and now it works fine.

Thanks for your help everyone!

6 replies

TDK
Sep 16, 2025 12:13 PM UTC

 

Probably a bug in the code somewhere else. The presented code looks fine.

Perhaps log register values to a debug stream so you can verify, or verify in debugging.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PhilippRAuthor
Associate
Sep 16, 2025 12:35 PM UTC

As I said, I already checked it in debugging. The value in the BRR definitly changes, but somehow the peripheral still uses the old configuration.

Andrew Neil
Super User
Sep 16, 2025 12:56 PM UTC

@PhilippR wrote:

The value in the BRR definitely changes, .


Maybe something changes it back ... ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PhilippRAuthorBest answer
Associate
Sep 16, 2025 2:37 PM UTC

I found the problem. The software which I used for testing the USART interface was not working as I expected it to do. So the baud rate of the controller was indeed configured back to the initial value. I modified the test software and now it works fine.

Thanks for your help everyone!