Skip to main content
Associate III
Nov 7, 2023 2:18 PM UTC
Solved

STM32WL_WS project don't build after changing configuration.ioc file

Hi all,

I have three STM32WL55 boards and I am following the STM32WL_WS Workshop tutorial. I can programmed one of the boards using SubGHz_Phy_Base_Station.bin and build the sensor SubGHz_Phy_PingPong project for the other two boards using the following \Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\P2P_Sensor.

Both Sensor board works fine and I can edit both the c code header files in the project and program them. However if I edit the SubGHz_Phy_PingPong.ioc file then the project stops to build.

Has any one else experience this issue. Many thanks in advance.

Regards

Ola

This topic has been closed for replies.
olaBest answer
Associate III
Nov 15, 2023 7:02 AM UTC

Hi STTwo-32,

The problem has now been resolved. The problem was that when the any changes was made to the  SubGHz_Phy_PingPong.ioc configuration file. The configuration wizard tools deletes most of the example code and leaves just a template code.

Regards

Ola 

5 replies

STTwo-32
ST Technical Moderator
Nov 13, 2023 9:49 AM UTC

Hello @ola and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Can you provide more information about the changes you have made on the SubGHz_Phy_PingPong.ioc so we can locate the problem better.

Best regards.

STTwo-32  

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
olaAuthorBest answer
Associate III
Nov 15, 2023 7:02 AM UTC

Hi STTwo-32,

The problem has now been resolved. The problem was that when the any changes was made to the  SubGHz_Phy_PingPong.ioc configuration file. The configuration wizard tools deletes most of the example code and leaves just a template code.

Regards

Ola