Skip to main content
ESchu.3
Associate
Oct 20, 2022 6:09 PM UTC
Solved

STM32WL V1.2.1 Application LoRaWAN Endnode How to reduce powerconsumtion in Stopmode 2? Now about 400µA expected 2µA!

..

This topic has been closed for replies.
Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Oct 28, 2022 3:29 PM UTC

Hello @Community member​ ,

I suggest you to try with the very simple examples under "Projects\NUCLEO-WL55JC\Examples\PWR" to verify your consumption. Like that you won't use the radio part that may lead to an over consumption

As you have the X-Nucleo-LPM01A Board, you can use STM32CubeMonitorPower software tool which is very useful to do current measurements.

Regards

Louis

4 replies

Piranha
Principal III
Oct 20, 2022 10:49 PM UTC
Louis AUDOLY
ST Employee
Oct 27, 2022 2:46 PM UTC

Hello @Community member​ ,

You mean STM32Cube_FW_WL_V1.2.0 ?

Which hardware are you using ?

How are you measuring this consumption ?

Regards

Louis

ESchu.3
ESchu.3Author
Associate
Oct 27, 2022 3:50 PM UTC

Hello Louis,

yes i mean STM32Cube_FW_WL_V1.2.0

The hardware is this one: RAK3272S Breakout Board | RAKwireless Documentation Center

The board itself has the RAK3172 at its core, integrating a STM32WLE5CC chip. It has Ultra-Low Power Consumption of 1.69 uA in sleep mode.

The low level development is descriped here: RAK3172 Module Low Level Development Reference | RAKwireless Documentation Center

I measuring the consumtion with the X-Nucleo-LPM01A Board and a digital multimeter.

Greetings

E_T

Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Oct 28, 2022 3:29 PM UTC

Hello @Community member​ ,

I suggest you to try with the very simple examples under "Projects\NUCLEO-WL55JC\Examples\PWR" to verify your consumption. Like that you won't use the radio part that may lead to an over consumption

As you have the X-Nucleo-LPM01A Board, you can use STM32CubeMonitorPower software tool which is very useful to do current measurements.

Regards

Louis