Skip to main content
Visitor II
Oct 9, 2026 12:52 PM UTC
Solved

STM32WL UFBGA73 – direct-tie (no RF switch) possible with RFO_LP only?

Hi all,

I'm designing a LoRa node with STM32WL55JCU6 (UFBGA73), using RFO_LP only (+14 dBm, high band 868 MHz). My starting point is the MB1842 reference design, which uses a BGS12SN6 RF switch between the TX and RX paths.

For UFQFPN48, ST provides direct-tie reference designs without a switch (MB1789). For UFBGA73, both MB1842 and MB1849 use an RF switch, and I couldn't find a direct-tie BGA73 reference.

Questions:
1. Is direct-tie recommended on UFBGA73 in LP mode?
2. Has anyone implemented it on BGA73? If so, what matching network did you use, and how did TX power and RX sensitivity compare to the switched design?
3. Are the TX/RX impedances for UFBGA73 available to design a direct-tie network per AN5457?

Thanks!

Imen.DBest answer
ST Technical Moderator
Oct 20, 2026 10:03 AM UTC

Hello ​@Jash and welcome to the Community,

There were indeed no reference designs in direct-tie configurations for the BGA package.
Below the optimal TX impedance and the optimal RX impedance for 868MHz 14dBm:

TX:Zopt = 17 +j* 21
 

RX:

Zsingle = 26 +j*52

Z_diff = 52 + j*104

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

4 replies

Imen.DBest answer
ST Technical Moderator
Oct 20, 2026 10:03 AM UTC

Hello ​@Jash and welcome to the Community,

There were indeed no reference designs in direct-tie configurations for the BGA package.
Below the optimal TX impedance and the optimal RX impedance for 868MHz 14dBm:

TX:Zopt = 17 +j* 21
 

RX:

Zsingle = 26 +j*52

Z_diff = 52 + j*104

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
Oct 28, 2026 9:38 AM UTC

Hello ​@Jash ,

I'm waiting for your feedback. 

When your question is answered, please close this topic by clicking “Best answer” button. This will help Community users find that answer faster.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Visitor II
Oct 28, 2026 10:07 AM UTC

Interesting design challenge. I’d be cautious about assuming the UFQFPN48 direct-tie network will translate to UFBGA73, since the RF layout and matching requirements may differ. Has ST confirmed whether BGA73 TX/RX impedance data is available for this setup?

ST Technical Moderator
Oct 28, 2026 4:00 PM UTC

Hi ​@jannybro ,

 

The impedance I provided earlier is related to the BGA73 package.

At the moment, there are no plans to optimize the BOM for this package without using an RF switch.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks