Skip to main content
Associate II
Jun 5, 2025 9:55 AM UTC
Solved

STM32WL - SUBGHZSPI DEBUG

For a project of mine, I wanted a LoRa Transceiver like (like the SX1262) to be controlled by a host application running on a STM32F4. I have a few STM32WLE5CCU6s lying around from a previous project, and was thinking if I could use them instead.

 

The SX1262 drivers are written in the host application, so I just need to access the actual transceiver's SPI and other signal lines.

 

I realize that the DEBUG option exposes critical pins like the SPI, NSS, RESET and BUSY. But are the DEBUG lines writeable or are they just for monitoring of signals?

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 3, 2025 1:47 PM UTC

Hello @MoralkaraLynn 

Radio is controlled internally through SUBGHZSPI and, for debug purpose only, from the external. So, the exposed options are used only for Debug.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jul 3, 2025 1:47 PM UTC

Hello @MoralkaraLynn 

Radio is controlled internally through SUBGHZSPI and, for debug purpose only, from the external. So, the exposed options are used only for Debug.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.