Skip to main content
Associate II
Jul 17, 2025 3:00 PM UTC
Question

STM32WL no Slave Reception on SUBGHZ SPI

Hi,

I am trying to set up a SPI communication to the STM32WL's integrated LoRa transceiver. So, I was able get NSS, MOSI and SCK to work, however I won't receive any data on the MISO line.

My code is following:

void SUBGHZSPI_DebugEnable(void) {
	RCC->AHB2ENR |= (1U << 0);		//enable GPIO-A

	GPIOA->MODER &= ~(3U << 8);		//reset PA4
	GPIOA->MODER |= (2U << 	8);		//set PA4

	GPIOA->MODER &= ~(3U << 10);	//reset PA5
	GPIOA->MODER |= (2U << 10);		//set PA5

	GPIOA->MODER &= ~(3U << 12);	//reset PA6
	GPIOA->MODER |= (2U << 12);		//set PA6

	GPIOA->MODER &= ~(3U << 14);	//reset PA7
	GPIOA->MODER |= (2U << 14);		//set PA7

	GPIOA->AFR[0] &= ~(15U<<16);	//reset AF of PA4
	GPIOA->AFR[0] |= (13U<<16);		//set AF13 of PA4

	GPIOA->AFR[0] &= ~(15U<<20);	//reset AF of PA5
	GPIOA->AFR[0] |= (13U<<20);		//set AF13 of PA5

	GPIOA->AFR[0] &= ~(15U<<24);	//reset AF of PA6
	GPIOA->AFR[0] |= (13U<<24);		//set AF13 of PA6

	GPIOA->AFR[0] &= ~(15U<<28);	//reset AF of PA7
	GPIOA->AFR[0] |= (13U<<28);		//set AF13 of PA7

	GPIOA->OSPEEDR |= (3U << 8);	//set output speed for PA4 to HIGH speed
	GPIOA->OSPEEDR |= (3U << 10);	//set output speed for PA5 to HIGH speed
	GPIOA->OSPEEDR |= (3U << 12);	//set output speed for PA6 to HIGH speed
	GPIOA->OSPEEDR |= (3U << 14);	//set output speed for PA7 to HIGH speed
}



void SUBGHZSPI_init(void) {

	 RCC->APB3ENR |= (1<<0); // enable SUBGHZ SPI

	 SUBGHZSPI->CR1 |= (1 << 9); // SSM
	 SUBGHZSPI->CR1 |= (1 << 8); // SSI

	 SUBGHZSPI->CR1 &= ~(7 << 3);
	 SUBGHZSPI->CR1 |= (1<<3); // baudrate (1MHz)

	 SUBGHZSPI->CR1 |= (1<<2); // Master
	 SUBGHZSPI->CR1 &= ~(1<<10); // full-duplex

	 SUBGHZSPI->CR2 |= (1<<12); // FIFO threshold 8bit

	 SUBGHZSPI->CR1 |= (1<<6); // enable SPI
}

 

I call this code in main.c by executing this:

while(1) {
		PWR->SUBGHZSPICR &= ~(1 << 15); // NSS low

		while (!(SUBGHZSPI->SR & (1 << 1))); // TXE
		*(__IO uint8_t*)(&SUBGHZSPI->DR) = 0x13;

		while (!(SUBGHZSPI->SR & (1 << 0))); // RXNE
		uint32_t status = SUBGHZSPI->DR;

		PWR->SUBGHZSPICR |= (1 << 15); // NSS high
	}

 

I can transmit data and can also verify with my logic level analyzer but the MISO line always stays high:

manuelambaum_0-1752764349546.png

Can anyone help me getting this running? Am I missing anythin?

 

Thanks in advance

 

This topic has been closed for replies.

3 replies

TDK
Jul 17, 2025 3:29 PM UTC

MISO is driven by the slave, not the master. What is it connected to?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
Jul 17, 2025 4:43 PM UTC

It is connected to the internal LoRa-Transceiver (Semtech SX126x). I configured the physical pins only for debugging purposes. I know that the MISO is driven by the Slave, I just can't influence the physical wiring since the SPI is internally wired.

STTwo-32
ST Technical Moderator
Aug 11, 2025 2:52 PM UTC

Hello @manuelambaum 

I should work fine if you apply the recommendations of this article.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.