Skip to main content
RPaja.1
Associate II
Apr 28, 2023 7:26 AM UTC
Question

STM32WL Memory definition in Lorawan_end_node

Hello,

I am developing my own project based on Lorawan_end_node project, i have some doubts regarding to memory addressing.

In linker file:

/* Memories definition */
MEMORY
{
 RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
 NVM_RAM (rw) : ORIGIN = 0x20008000, LENGTH = 4K
 RAM2 (xrw) : ORIGIN = 0x20009000, LENGTH = 28K
 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 248K
 USER_Key_region_ROM (rx) : ORIGIN = 0x0803E500, LENGTH = 768
}

I don not unsdestand NVM_RAM section, what is it? and USER_Key_region_ROM?

I am trying to optimizate LoRaWAN NVM Context save proccess in FLASH. By default it is saved in

#define LORAWAN_NVM_BASE_ADDRESS          ((void *)0x0803F000UL)

It would be the last two pages(2x2kB) of flash memory in case FLASH memory LENGTH  would be 256K as expected..

Normally, another section would be present, something like this

USER_FLASH (rx) : ORIGIN = 0x0803F000UL , LENGTH = 4K

Can someone help me to undestand this?

Regards,

This topic has been closed for replies.

1 reply

IIRHO.1
ST Employee
Apr 28, 2023 3:32 PM UTC

Hello @RPaja.1​   and welcome to ST Community.

I advise you to check these resources :

hope this is helpful

Issam

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.