Skip to main content
RLind.3
Associate III
Sep 6, 2022 8:59 PM UTC
Solved

STM32WL CFO Registers

Hi there,

I am using an STM32WLE4C8 with FSK and I am trying to determine the offset between the internal carrier frequency and an incoming carrier frequency. This offset will be used to calibrate my device using a high accuracy incoming preamble and sync word.

I believe I should be using the CFO registers of the radio (0x06B0 and 0x06B1), based on the function SUBGRF_GetCFO() in radio_driver.c from Semtech. However, I am getting wildly varied results from this function, even after averaging the samples. Repeated tests have resulted in sample variation of up to 10kHz.

Unfortunately, there is minimal documentation on these CFO registers. They are mentioned in RM0461 with the description "actual frequency error from normalized value". They aren't mentioned at all in the SX126x datasheet.

Has anyone successfully used the CFO registers before? Or have any ideas for getting a reliable offset reading? Due to the lack of documentation, I am not quite sure how to use them correctly.

Thanks,

Rebecca

This topic has been closed for replies.
Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Sep 7, 2022 7:57 AM UTC

Hello Rebecca,

This bug has already been fix and will be available in the next release, you have to modify the function SUBGRF_GetCFO, and to replace the line :

uint32_t cf_fs = XTAL_FREQ / ( bandwidth_mant * ( 1 << ( bandwidth_exp - 1 )));

by the line :

uint32_t cf_fs = XTAL_FREQ / ( bandwidth_mant * ( 1 << ( bandwidth_exp + 1 )));

I hope my answer helped you!

When your question is answered, please close this topic by choosing Select as Best.

Regards

Louis

2 replies

Louis AUDOLY
Louis AUDOLYBest answer
ST Employee
Sep 7, 2022 7:57 AM UTC

Hello Rebecca,

This bug has already been fix and will be available in the next release, you have to modify the function SUBGRF_GetCFO, and to replace the line :

uint32_t cf_fs = XTAL_FREQ / ( bandwidth_mant * ( 1 << ( bandwidth_exp - 1 )));

by the line :

uint32_t cf_fs = XTAL_FREQ / ( bandwidth_mant * ( 1 << ( bandwidth_exp + 1 )));

I hope my answer helped you!

When your question is answered, please close this topic by choosing Select as Best.

Regards

Louis

RLind.3
RLind.3Author
Associate III
Sep 7, 2022 7:49 PM UTC

Thanks Louis, this fixed my problem and I can now calibrate my device successfully! Thank you! :smiling_face_with_smiling_eyes: