Skip to main content
Associate
Oct 22, 2026 12:20 AM UTC
Solved

STM32WL – Can TX and TX_HP use separate matching networks at different frequencies with one shared antenna, without an RF switch?

Hello,

 

I am designing a circuit using the STM32WL3R with a single shared antenna for two transmit frequencies.

 

My requirements are:

- 315 MHz: TX output, low RF power (approximately -40 dBm)

- 433 MHz: TX_HP output, high RF power (approximately +12 dBm)

- One shared antenna

- Separate matching networks for 315 MHz and 430 MHz

 

I would like to avoid an external RF switch if possible.

 

1. Can both matching networks be permanently connected to the shared antenna feed point, while enabling only one PA path at a time?

2. When TX is transmitting at 315 MHz, what is the RF impedance of the disabled TX_HP output? Can the TX_HP output and its matching network affect the 315 MHz matching?

 

I would appreciate any recommendations regarding the RF topology and matching network design.

 

Thanks.

 

Imen.DBest answer
ST Technical Moderator
Nov 6, 2026 11:24 AM UTC

Hi ​@Ryo T 

Thank you for sharing the details.

We suggest using only the 433 MHz matching network, connecting only TX_HP, to also operate at 315 MHz, since the required power is very low, around -40 dBm.

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

ST Technical Moderator
Nov 5, 2026 3:22 PM UTC

Hello ​@Ryo T and welcome to the Community,

Could you please provide more details about the final application and what is expected?

Why you need to use two different matching networks, since the TX power wants to achieve at 315 MHz is very low (-40 dBm): moreover, the matching network we suggest in our 315MHz reference designs is optimized for power up to +16 dBm.

We advise you using only the network optimized for 433 MHz and evaluate the RF performance at 315 MHz. In this way, you can save on BOM cost and also optimize the PCB size.

Do you want to use only the TX path, or would you also to use the RX path?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Ryo TAuthor
Associate
Nov 6, 2026 1:24 AM UTC

Thank you for your reply.

Our application requires both 315 MHz and 433 MHz operation on a single PCB, with different output power levels for each frequency due to different regulatory requirements.

Our intended configuration is:

  • 315 MHz: Low output power, using the TX path.

  • 433 MHz: Higher output power (approximately +12 dBm), using the TX_HP path.

  • RX: We also need to use the RX path.

  • Both frequency bands share a single monopole antenna.

My idea was to assign 315 MHz to the TX path and 433 MHz to the TX_HP path, and switch between them by software configuration, without using an external RF switch.

Regarding your suggestion to use only the matching network optimized for 433 MHz, I would like to clarify the following:

If we use a single 433 MHz matching network, can both the TX and TX_HP paths remain permanently connected to the same antenna, without an external RF switch?

In other words, when operating at 315 MHz, we would transmit through the TX path, and when operating at 433 MHz, we would transmit through the TX_HP path. The unused TX path would remain connected to the antenna.

Would this configuration cause any problems, such as impedance mismatch, RF signal leakage into the unused path, or degradation of TX/RX performance?

Is this configuration supported by the STM32WL3R internal RF architecture?

Thank you for your advice.

Imen.DBest answer
ST Technical Moderator
Nov 6, 2026 11:24 AM UTC

Hi ​@Ryo T 

Thank you for sharing the details.

We suggest using only the 433 MHz matching network, connecting only TX_HP, to also operate at 315 MHz, since the required power is very low, around -40 dBm.

Hope this helps!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks