Skip to main content
edmond yun
Associate III
Nov 21, 2024 1:26 AM UTC
Solved

STM32WL build error with CubeMX & IAR

HI, 

please help to check the following build error.

I used CubeMX and IAR build tool and the following code.

en.stm32cubewl-v1-3-0\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node

 

Error is as below,

Error[Li005]: no definition for "BSP_RADIO_GetRFOMaxPowerConfig" [referenced from C:\work\stm_project\Lora_Test\
WLE5CC6_LORA\EWARM\WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_GetTxConfig" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\
EWARM\WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_ConfigRFSwitch" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\
EWARM\WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_IsDCDC" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\EWARM\
WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_Init" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\EWARM\
WLE5CC6_LORA\Obj\radio_board_if.o]
Error[Li005]: no definition for "BSP_RADIO_IsTCXO" [referenced from C:\work\stm_project\Lora_Test\WLE5CC6_LORA\EWARM\
WLE5CC6_LORA\Obj\radio_board_if.o]
Error while running Linker

Total number of errors: 6

 

thanks.

This topic has been closed for replies.
edmond yun
edmond yunBest answer
Associate III
Jan 15, 2025 12:16 AM UTC

Hi, 

I solved with importing official DK board setting.

thankful for your concern.

thanks.

2 replies

STTwo-32
ST Technical Moderator
Nov 21, 2024 8:10 AM UTC

Hello @edmond yun 

I'm not able to reproduce this issue using the STM32CubeWL V 1.3.0, STM32CubeMX V6.12.1 and EWARM V9.60.2. Could you please update to those versions and ensure to download the SDK from our ST website.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
edmond yun
edmond yunAuthorBest answer
Associate III
Jan 15, 2025 12:16 AM UTC

Hi, 

I solved with importing official DK board setting.

thankful for your concern.

thanks.