Skip to main content
Associate II
Jun 25, 2025 4:06 AM UTC
Question

STM32WBDK LPM wont allow PWM to work

 

I’m driving a hobby servo on the STM32WB5MM-DK Discovery board using TIM2 PWM and the STM32CubeWB Sequencer/LPM utilities. When I disable low-power mode entirely, the servo moves flawlessly on each 500 ms button-hold toggle. But as soon as I allow the LPM manager to enter Stop mode, the PWM pulses become unstable and the servo either jitters or stops moving.

PWM in Stop Mode: Are there proven techniques to retain stable PWM outputs during Stop or Low-Power Run modes on STM32WB series?

Sequencer Integration: Can anyone share examples of driving servos reliably while staying in LPM using the Utility Sequencer?

I have uploaded the project. 

 

This topic has been closed for replies.

3 replies

FilipKremen
ST Employee
Jun 25, 2025 6:24 AM UTC

Hello,

if you want to generate a PWM signal in LP mode, you could use a LP timer.

Please kindly read section 27 in RM.

Multiprotocol wireless 32-bit MCU Arm<Sup>®</Sup>-based Cortex<Sup>®</Sup>-M4 with FPU, Bluetooth<Sup>®</Sup> Low-Energy and 802.15.4 radio solution - Reference manual

If you have any other question, please let me know.

Best regards,

Filip Kremen

Associate II
Jun 25, 2025 7:14 AM UTC

I was expecting to have better control over the application as in not enter low power mode before the button event is set. Could you please have a look at my application code and suggest me a way to do so.

FilipKremen
ST Employee
Jun 25, 2025 12:16 PM UTC

Hello,

I have quickly checked your project, can you please try to move UTIL_LPM_SetStopMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE) function at the end of PWM_timer_ISR()? This will enable stop mode after stopping the PWM signal.

Best regards,

Filip Kremen