Skip to main content
Associate II
Mar 5, 2026 12:00 PM UTC
Solved

STM32WBA5MMG GND pads near antenna

Dear all,

I have a custom PCB with the STM32WBA5MMG module. I missed the keepout requirement in the reference design and pads 2 - 5 and pads 56 / 59. These pads are connected to GND in my design. I did some signal tests, and I have a feeling the antenna is not performing well (I configured +10dbm).

Can somebody confirm these pads connected to ground influence the antenna performance? Below is a snippet of the PCB design:image.png

 

Thanks,

Robin

XERC
XERCBest answer
ST Employee
Mar 5, 2026 4:55 PM UTC

Hello, yes clearly the keep out requirement is important to have optimal antenna performance. This should be applied on all layers. This is difficult to estimate precisely what is the real impact in term of performances, but there will be degradation for sure on both Tx and Rx.

 

1 reply

XERC
XERCBest answer
ST Employee
Mar 5, 2026 4:55 PM UTC

Hello, yes clearly the keep out requirement is important to have optimal antenna performance. This should be applied on all layers. This is difficult to estimate precisely what is the real impact in term of performances, but there will be degradation for sure on both Tx and Rx.