Skip to main content
Associate III
Jan 14, 2026 6:21 AM UTC
Question

STM32WBA55 + BLE_p2pServerThreadX: Firmware does not start after Power-On Reset, only runs after manual Reset

Hello ST Community,

I am working with NUCLEO-WBA55CG and encountering a startup issue when using the BLE_p2pServerThreadX example from STM32CubeWBA v1.8.0.

Environment

  • Board: NUCLEO-WBA55CG

  • MCU: STM32WBA55 (single-core Cortex-M33)

  • SDK: STM32CubeWBA v1.8.0

  • RTOS: Azure RTOS ThreadX

  • Example: BLE_p2pServerThreadX

  • IDE / Toolchain: IAR Embedded Workbench 9.60

  • Debugger: ST-LINK (on-board)

Problem Description

After programming the firmware to the board:

  • :cross_mark: On cold power-on (Power-On Reset), the application does not start

  • :white_heavy_check_mark: After pressing the RESET button, the application runs normally

  • The issue is 100% reproducible

BLE advertising starts correctly only after a manual reset, not after initial power-up.

 

Additional Tests Performed

  • The issue occurs even when Timebase Source is set to SysTick

  • The MCU is confirmed to be STM32WBA55 (single-core)
    (not STM32WB, no wireless coprocessor)

  • No user code is executed after early initialization during the failing POR case

  • After RESET, behavior is normal without any code changes


Debug Observations

During the failing Power-On Reset case:

  • HAL_GetTick() always returns 0

  • SysTick interrupt does not appear to be running

  • BLE initialization seems to stall during early startup (likely in timebase-dependent code paths)

During the RESET case:

  • SysTick is correctly enabled

  • HAL_GetTick() increments as expected

  • BLE stack initializes and advertises normally

This strongly suggests that SysTick is not properly enabled or reinitialized after POR, possibly due to the interaction between:

  • HAL_Init()

  • ThreadX low-level initialization

  • BLE initialization using HAL timebase–dependent APIs (e.g. HAL_Delay() or timeout loops)


Suspected Root Cause

This appears to be a startup sequencing issue specific to Power-On Reset when using:

  • CubeWBA v1.8.0

  • ThreadX

  • IAR 9.60

SysTick may be left disabled or misconfigured after POR, while a manual RESET correctly reinitializes NVIC and SysTick state.


Questions

  1. Is this a known issue in STM32CubeWBA v1.8.0 with ThreadX projects?

  2. Is there an official workaround or patch recommended by ST?

  3. Should SysTick be explicitly reconfigured before tx_kernel_enter() in WBA ThreadX applications?

  4. Has this issue been fixed in a later CubeWBA release?

Any confirmation or guidance would be greatly appreciated.

Thank you for your support.