Skip to main content
agnes
Associate II
Oct 6, 2025 2:16 PM UTC
Solved

STM32WBA54KGU6 - SMPS code generated...

Hi Champs,

one of my customers develop on STM32WBA54KGU6. This SoC does not come with SMPS.

Although he selects the righ reference (STM32WBA54KGU6) for code generation, SMPS seems to be used by default - he has to comment the line out form generated code to build properly.

he uses the latest dev tool versions :

  • IDE : STM32CubeIDE V1.19.0
  • Firmware  STM32CubeWBA : V1.7.0

is it a known issue?

please note that it is not a blocking point but it still requires a post code generation control from his side to comment out the generated SMPS statement in the generated code.

Warm regards, Agnès

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Oct 9, 2025 6:29 AM UTC

Hello All,

Thank you for having reported this issue

I escalated this request internally for fix (ticket number: 219199)
(PS: ticket number: 219199 is an internal tracking number and not available outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

7 replies

STTwo-32
ST Technical Moderator
Oct 6, 2025 3:14 PM UTC

Salut @agnes 

Could you please attach the .ioc file of your customer (or send it as a privet message). There is not a known issue about SMPS code generation for the STM32WBA54.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
agnes
agnesAuthor
Associate II
Oct 8, 2025 3:46 PM UTC

hello ,

here  attached you might find the .ioc files + the whole project in case you need.

Warm regards,

Agnès

Issamos
Super User
Oct 8, 2025 5:33 PM UTC

Hello @agnes 

According to the .ioc file it seems to select the PWR_SMPS_SUPPLY as RCC supply source. I think ST should solve this problem. Since the STM32WBA54 family is a LDO MCU without SMPS support. @STTwo-32 @Imen.D could you please check and report this.

Best Regards.

STTwo-32

Imen.DBest answer
ST Technical Moderator
Oct 9, 2025 6:29 AM UTC

Hello All,

Thank you for having reported this issue

I escalated this request internally for fix (ticket number: 219199)
(PS: ticket number: 219199 is an internal tracking number and not available outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Visitor II
Oct 9, 2025 9:12 AM UTC

It seems this is a known behavior with STM32CubeIDE code generation for STM32WBA54 devices. You may want to this related discussion for more details and possible workarounds: 

https://community.st.com/t5/stm32-mcus/visit-stm32cubeide-smps-configuration-issue/td-p/832475

ST Technical Moderator
Oct 20, 2025 12:29 PM UTC

Hello @agnes ,

Were you able to resolve the issue with my attached ioc file?

Do you agree with my assessment, or is there anything you would like to add?

I will wait for your feedback.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks