Associate III
Oct 30, 2024 1:40 PM UTC
Question
STM32WBA52 LSE as GPIO Issue
- 4 replies
- 1941 views
Hi,
Requirement: Use LSE pins: PC14/PC15 as GPIO Output.
MCU: STM32WBA52CGU6
Issue: Output voltage not sustain at 3.3V but getting 3.152V (GPIO connected circuit consumes 300uA only).
- For clean firmware, generated firmware based on IOC, configured only these two pins as output, push-pull, High state.
- Attached related IOC-file, debug-SFR-states-screenshot and generated-project files.
I thinks that this is STM MCU level limitation and STM-Team must provide errata for same with workaround-status.
Please guide me in case anyone have known workaround.
Thanks