Skip to main content
SWenn.1
Senior III
Sep 4, 2023 6:50 PM UTC
Solved

STM32WB5MMGH6TR BLE Question on Pairing ....using MOOC video???

Hello all..

I have a proprietary pcb with the above mcu.  Board works fine.  I am using BLE but with NO bells and whistles (no encryption, authenication or authorizations.  I decided I wanted to play around with these things so I have been following the MOOC videos on security.  In the following video at 3:12

MOOC Pairing video 

the presenter shows that a pairing window pops up on the screen.  I have done exactly what he has done in short the only change I make is to change a NO to a YES on one of the characteristic permissions for ENCRYPTION READ.  When I try and access this my phone applications (I've tried nRFConnect and ST BLE Toolbox) disconnects and I do NOT get any pairing message.  Other characteristics seem to work fine.  Can anyone tell me what I may have wrong here?  

I am using a power supply so no current limit issues and the parameter can be read fine when I turn YES back to NO.

Thanks

Steve

This topic has been closed for replies.
SWenn.1
SWenn.1Best answer
Senior III
Sep 8, 2023 2:51 PM UTC

As I've said before I did that....it does not work...app disconnects....

Turns out the key which was never mentioned was setting

CFG_MITM_PROTECTION to MITM protection not required (0x00)

5 replies

Issamos
Super User
Sep 4, 2023 10:23 PM UTC

Hello @SWenn.1 

For the Hands-on Pairing Just works, Characteristic must require encryption before it can be read by Client. Upon read request, GATT server will generate error message “Insufficient Encryption”. Client will then initiate pairing and encrypt the link.

You shall not require Authentication since there is no MITM protection with Just Works.

Best regards.

II

SWenn.1
SWenn.1Author
Senior III
Sep 5, 2023 5:02 PM UTC

Hello II

if you mean set the parameter as below I already done that as the video explains this....If you mean some other switch needs to be set somewhere then please point me to the correct tab /location as the video definitely does NOT suggest anything else

 

SWenn1_0-1693933366701.png

 

Issamos
Super User
Sep 5, 2023 5:53 PM UTC

Hello again

Yes, I mean set the parameter as you have done. To make the application work you need to switch ENCRYPTION READ to Yes.

Best regards 

SWenn.1
SWenn.1AuthorBest answer
Senior III
Sep 8, 2023 2:51 PM UTC

As I've said before I did that....it does not work...app disconnects....

Turns out the key which was never mentioned was setting

CFG_MITM_PROTECTION to MITM protection not required (0x00)

RPowe.1
Associate II
Apr 3, 2025 1:53 PM UTC

Was this ever solved? I am trying the same thing and getting the same result as SWenn.1.
Following the video "BLE Security with STM32WB - 05 Pairing - just works lab", https://www.youtube.com/watch?v=j-d7SY2BL3I. My settings are as below. When I try to read the characteristic, instead of prompting to pair, it disconnects.

From Teraterm:, I get this...

>>== ACI_GAP_PAIRING_COMPLETE_VSEVT_CODE

- Pairing KO

- Status: 0x1

- Reason: 0x0

>>== HCI_DISCONNECTION_COMPLETE_EVT_CODE

- Connection Handle:   0x803                                                                                                                                                                          - Reason:    0x13

RPowe1_0-1743687997133.png

RPowe1_1-1743688027863.png