Skip to main content
Associate III
Jul 31, 2025 7:15 AM UTC
Question

STM32WB5MMGH6TR and STM32WL5MOC on the same board

Hi,

I want to integrate on the same PCB both a STM32WB5MMGH6TR and a STM32WL5MOC. Are there any issue in terms of RF interference? Are there any shielding recommendations to avoid problems while both modules are transmitting?

Thanks

Matteo

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
Jul 31, 2025 8:08 AM UTC

Most (all?) of the issues would be generic to co-locating any sub-GHz radio with any 2.4GHz radio - not specific to STM32.

So have you tried a general internet search on that?

eg, look at Amazon Sidewalk ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
STTwo-32
ST Technical Moderator
Sep 10, 2025 4:03 PM UTC

Hello @matteverze 

As said @Andrew Neil, the interference issue is the same for all the products that include two communication modules working on different band. So, the recommendation is to always keep signal isolation between both modules. More information may be found everywhere on the web. You may also refer to the design of the STEVAL-ASTRA1B that is based on the STM32WB5MMG module and the STM32WL55JC (MCU used for the STM32WL5MOC.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.