Skip to main content
Visitor II
Oct 30, 2025 12:27 PM UTC
Question

STM32WB5MMG with Full BLE stack / Power Consumption

Hi All,

I'm currently using an STM32WB5MMG on my project and I'm struggling to reach the expected power consumption.

Please note one known error on the PCB: the RF_OUT and ANT_IN pins, which should be connected to GND according to the datasheet/guidelines, were inadvertently left unconnected. These pins are currently inaccessible for rework.

Anyway, I'm trying with all the examples available for this MCU, and I have read all the conversations about this MCU and the Low Power modes multiple times with no success.

I have tested the PCB with the HeartRateFreeRTOS example and with the PWR_STOP2_RTC example, but again, no luck.

The current is always around 500 μA.

I have already tried to desolder all the sensors from the PCB to be sure that the extra consumption doesn't come from one of them, but no luck.

I have also deactivated all debug functionality while testing for power consumption, and I have tested the PCB with the debugger disconnected, so it is not related to this.

I also tried to initialize all the GPIO as ANALOG input as suggested in some posts (in PWR_STOP2_RTC, it was already done, so this is not the problem)

 

My First question is:" Could the missing connection to GND of RF_OUT and ANT_IN cause the extra consumption ?" I have no way to test this because those pins are not reachable to try to do a rework.

 

Second question: If this is not the issue, is there any known problem that could lead to this anomalous consumption?

Thanks
Jonny 

This topic has been closed for replies.